Automotive power distribution topologies are undergoing a dramatic change as domain-based vehicle architectures shift towards zone-based architectures. At the same time zonal control modules are increasingly adopting semiconductor switches for power distribution wire harness protection replacing melting fuses that are the dominant protection elements today. The main semiconductor switch benefits include:
The transition from melting fuses to semiconductor switches is shown in Figure 1
There are a number of challenges to overcome in semiconductor high side switches when used as smart fuse devices. These include lowering the quiescent current with the switch in the ON state and turning on outputs powering large capacitive loads typically seen at the load (Electronic Control Unit (ECU) input). Further, zone control modules and Input-Output (IO) Aggregator ECUs usually power a large variety of ECUs and actuators making the design and development a challenge. Texas Instruments is introducing a new portfolio of smart high side switches with integrated FETs and a wide Ron range addressing these concerns. The TPS2HCS10-Q1 device is the first fully software configurable device in the market that comprehensively addresses the development and technical challenges. The device incorporates all of the specific features needed for a power distribution switch as well as the traditional protective and diagnostic functions seen in high side switches for actuator drive applications.
This application brief shows how a software configurable device enables platform design of zonal controller modules as a part of the general trend where the zonal architecture paves the way to a fully software-defined vehicle. Next we discuss how the SPI configurable TPS2HCS10-Q1 device meets all the requirements like programmable fuse characteristics and low quiescent current and designed for driving any type of load-capacitive ECU loads or resistive/inductive actuator loads.
The TPS2HCS10-Q1 device uses an SPI serial interface from the MCU to configure the device based on the load requirements and to read the load diagnostics. The many advantages of a software configurable switch include:
A single platform development can suffice for the various automotive model variants with different output load characteristics. The development and validation effort is thus simplified, thus enabling a faster time to market and lower development and validation cost.
The TPS2HCS10-Q1 includes an embedded fuse characteristic time-current curve to determine when/if the switch turns off depending on the time/duration of the load current. This feature enables the device to pass high load currents for brief period (motor inrush and stall currents, for example), yet turn-off under overload conditions to protect the wire harness, PCB traces and connectors. The device can be compared to a melting fuse but with significantly tighter part-part variation. Further, SPI configuration in TPS2HCS10-Q1 enables a large programming range for fuse curves with just two key parameters, the nominal current and the shut-off energy trigger threshold. The nominal current is roughly equivalent of the melting fuse current rating matching DC current capability of the wire. However, unlike a melting fuse, the device offers additional options to program multiple choices of the time-current curve for a given nominal current rating. This wide range is available for each on-resistance (RdsON) variant of the device family. The fuse time-current curve is then combined with a configurable delayed turn-off current based on the ADC current sense and a very fast turn-off for short circuit protection.
The overall protection scheme across the full current range is shown in Figure 3. The figure also shows how to choose the fuse curve from the programmable choices, to meet the requirements for wire protection while allowing all normal load transients to pass through.
There are quite a large number of ECUs that need to be powered even while the vehicle is in a park (key-off) state. Additionally, the switch that is providing power to these ECUs needs to consume very low operating current while the switch is in the ON state and providing a small amount of load current. Yet the load can demand tens or even hundreds of mAs of peak current for a short time (and low duty cycle) while performing monitoring functions. The goal of the power distribution switch is to operate in a low quiescent mode providing the peak current and when the load demands a current in excess of the peak current, switch over to the normal operation mode and signal this to the MCU.
The TPS2HCS10-Q1 device has been designed to meets all of these key requirements of the power on at all times (PAAT) switch application.
A key benefit of a fully software configurable device is that the device can be tailored to drive large capacitive loads seen on ECU loads. The device can be configured in the capacitive charging mode that is the best choice for the capacitance and the parallel load current draw. The device offers two options, a constant current charging mode designed for cases where there is a significant load current during charging phase or a fixed dV/dt rate charging mode that is designed for very large capacitive loads that needs to be charged with a very low charging current. In either case, the inrush current is limited to a low value during a programmable charging duration. A view of the charging and load current drive behavior is shown in Figure 5. All elements of cap charging including charging current (or dV/dt rate), charging duration and type are configurable over SPI.
The document highlights the key benefits of the new TPS2HCS10-Q1, the first fully software configurable smart high side switch in the market. The device enables rapid platform development and improves time to market, at the same time solving a number of challenges seen in the transition from melting fuse wire harness protection to semiconductor switches, Table 1 provides an overview of the key features and the system benefits that these features provides.
Features | TPS2HCSxx-Q1 Integrated FET Smart eFuseHigh Side Switch | System Benefit |
---|---|---|
MCU Interface | Daisy Chainable SPI HSS | Fully software configurable (tailored to each output load). Maximum load and fault diagnostics without external components enabled by SPI |
Low Quiescent current mode, System wake | Peak current capability of up to 1 A ( in key-off state) and programmable wake threshold. Iq < 10µA/ch max from battery supply VBB with both channels ON | Low Iq and higher current capability with no external components or FETs. Device can transition to low power mode to reduce current consumption in ACTIVE state as well as have programmable wake thresholds. The device generates a WAKE_SIG to wake the MCU upon load current increase. |
Cap charging | Slow ramp dV/dt or current limitation. cap charging modes. High (> 2mF) cap charging ability with constant current loads. | Configure loads as capacitive or actuator and associated inrush profiles. No limitation on number of cap charge cycles. No MCU overhead to enable charging mode and to time the charging mode after initial configuration |
Over-current Protection | Over-current protection thresholds programmable in SPI. Dual thresholds for inrush current. | Reduce supply droop during short circuit. No external components to set the threshold. |
I2t Overload Protection | Digital and programmable, no external components (lower variability) | Fully programmable fuse Time-Current curve and low variability wire protection enables lighter harness with no MCU involvement. No MCU monitoring current across multiple channels simplifies software, and full protection even with MCU failure. |
Diagnostics to aid Functional Safety | Digital Current, VOUT, Vds diagnostics | VOUT/VDS ADC measurement for better load diagnostics. Very accurate low current sensing for leakage / open load diagnostics (using offset/leakage trim capability) with built-in ADC. Open-load / short to supply and FET-short failure detection with no external components. |