SLVAFP0 December 2023 LMR51610
Focused on light loading application the designed inductor current ripple is 20% to 40% the inductor average current ,and the total loading with 100mA as example, show SCH in the following.
Notice the current limit is 1.6A for LMR51610. And the max Iout can support for IBB use Equation 7. KIND is a coefficient that represents the amount of inductor ripple current relative to the maximum output current of the device, usually K=0.2 – 0.4. IOUT_IC = 1A for LMR51610. Dnorm = 0.38 at VIN_norm = 24V, K=0.4, fsw = 400khz, result L=56uH.
The LMR51610 is protected from over-current conditions by cycle-by-cycle current limit. To prevent inductor saturation in case of short circuit conditions, the inductor saturation current needs to be greater than the device maximum peak current limit.