SLVAFP0 December 2023 LMR51610
The output current capability in the IBB topology is less than the buck configuration. This is because the inductor average current is different from Buck technology, that in buck circuit inductor current is the same as Iout current. As a result, refer to the following equations to choose the device to cover inductor max current in IBB use.
In Equation 4, where IOUT is the maximum output current of the device (IOUT = 1A). The inverting power supply output current limit is calculated as shown in Figure 7-2.Where D is duty cycle of IBB , and take consider the η= 80% for efficiency in Equation 3.
VO (V) | VIN (V) |
η |
D |
IOUT (A) |
---|---|---|---|---|
-12 |
24 |
0.8 |
0.38 |
0.61 |
-5 |
24 |
0.8 |
0.20 |
0.79 |
-15 |
24 |
0.8 |
0.43 |
0.56 |