SLVAFT2A May 2024 – July 2024 TPS2HCS10-Q1
Puts the device into LPM mode.
This function can send the command to go into LPM mode. The MCU is responsible to monitor the FLT pin for a falling edge if the exit current if the device exceeds the exit current level. Alternatively, the HCS_wakeupDevice function can be used to wakeup the device.
in | ch1ExitCurrent | Exit current for channel 1 |
in | ch2ExitCurrent | Exit current for channel 2 |