SLVAFW9 August 2024 LM51772
The current monitor (IMONLIM) function can be enabled when operating power stages in parallel and being used in multiple options. With two power stages, the following options are possible:
The configuration with the current monitor on the input and the current monitor on the output is shown in Figure 3-1.