SLVAFW9 August 2024 LM51772
With the results from the previous section, parallel operation using LM51772 converters can be done with a load sharing within 10% relative error. As per inductor current, a favorable synchronization between the phases can be seen with a slight variation in peak current value, which can be compensated by using a similar inductor. Additionally, the results from the thermal tests also confirm the thermal stability of the converters in a parallel fashion, but a slightly high temperature is measured for the boost region in comparison to the buck and buck-boost region. Moreover, the thermal comparison among single-phase and dual-phase operations confirms the high thermal efficiency and low losses in dual-phase operation.