SLVK117 October 2022 TPS7H2221-SEP
SETs are defined as heavy-ion-induced transients upsets on VOUT of the TPS7H2221-SEP. The species used for the SET testing was a Xenon (129Xe) ion and a Silver (109Ag) with an angle-of-incidence of 0° for an LETEFF = 42.7 and 46.8 MeV·cm2/mg, for more details refer to Section 5. Flux of approximately 104 ions/cm2·s and a fluence of approximately 3 × 106 ions/cm2 were used for the ten 129Xe SET runs. Flux of approximately 105 ions/cm2·s and a fluence of approximately 107 ions/cm2 were used for the six 109Ag SET runs.
VOUT SETs were characterized using a window trigger of ±3% around the nominal output voltage. The devices were characterized at VIN = 1.8-V, 3.3-V, and 5-V. The output load was set to either 100-mA, 500-mA, or 1.25-A using a Chroma E-Load in constant resistance (CR) mode. To capture the SETs an NI-PXIe-5172 scope card was used to continuously monitor the VOUT. The output voltage was monitored by using the TP2 (U1) and the TP7 (U2) test points on the EVM. The scope triggering from VOUT was programmed to record 50k samples with a sample rate of 10 Mega samples per second (MS/s) in case of an event (trigger). The scope was programmed to record 20% of the data before (pre) the trigger.
Under heavy-ions, the TPS7H2221-SEP exhibits transient upsets that were fully recoverable without the need for external intervention.Test conditions and results are summarized in Table 8-1. Histograms for the VOUTSET transient time are shown in Table 8-1. There is no histogram for the VOUTSET peak percentage as all SETs dropped to 0-V before fully recovering as shown in the worst case transient image.Table 8-1 shows typical time domain plots for all of the observed SETs.
Note that for the SET cases where the 109Ag ion was used, the total fluence per run was over 3 times as long as the runs with 129Xe which accounts for the increase in number of transients per run.
RUN # | UNIT # | ION | LETEFF(MeV·cm2/mg) | FLUX(ions·cm2/mg) | FLUENCE (# ions) |
VIN(V) | LOAD (A) | VOUTSET (#) ≥ ±3% |
---|---|---|---|---|---|---|---|---|
16 |
1 | 129Xe | 42.7 | 1.12 × 104 | 3 × 106 |
1.8 |
0.1 |
142 |
17 |
1 |
129Xe | 42.7 | 1.15 × 104 | 3 × 106 |
3.3 |
0.1 |
126 |
18 |
1 |
129Xe | 42.7 | 1.13 × 104 |
3 × 106 |
3.3 |
1.25 |
116 |
19 |
1 |
129Xe | 42.7 |
1.21 × 104 |
3 × 106 |
5 |
0.1 |
112 |
20 |
1 |
129Xe | 42.7 | 1.10 × 104 |
3 × 106 |
5 |
1.25 |
98 |
21 |
2 |
129Xe | 42.7 | 1.19 × 104 | 3 × 106 |
1.8 |
0.1 |
138 |
22 |
2 |
129Xe | 42.7 | 1.15 × 104 | 3 × 106 |
3.3 |
0.1 |
113 |
23 |
2 |
129Xe | 42.7 | 1.13 × 104 | 3 × 106 |
3.3 |
1.25 |
130 |
24 |
2 |
129Xe | 42.7 | 1.20 × 104 | 3 × 106 |
5 |
0.1 |
103 |
25 |
2 |
129Xe | 42.7 | 1.10 × 104 | 2.99 × 106 |
5 |
1.25 |
106 |
26 |
3 |
109Ag |
46.8 |
1.08 x 105 |
9.94 x 106 |
3.3 |
1.25 |
395 |
27 |
3 |
109Ag | 46.8 | 1.08 x 105 |
1 x 107 |
5 |
1.25 |
321 |
28 |
3 |
109Ag | 46.8 | 1.03 x 105 | 9.95 x 106 |
1.8 |
.5 |
472 |
29 |
4 |
109Ag | 46.8 | 1.11 x 105 | 9.98 x 106 |
3.3 |
1.25 |
377 |
30 |
4 |
109Ag | 46.8 | 1.02 x 105 | 9.99 x 106 |
5 |
1.25 |
329 |
31 |
4 |
109Ag | 46.8 | 1.09 x 105 | 9.98 x 106 |
1.8 |
.5 |
451 |
Using the MFTF method described in Single-Event Effects (SEE) Confidence Interval Calculations application report, the upper-bound cross section (using a 95% confidence level) is calculated for the different SETs as shown in Table 8-2 and Table 8-2 .
SET TYPE |
ION |
VIN (V) |
# UPSETS | UPPER BOUND CROSS SECTION (cm2/device) |
---|---|---|---|---|
VOUTSET ≥ |3%| |
129Xe |
1.8 |
280 |
5.25 x 10-5 |
VOUTSET ≥ |3%| | 129Xe |
3.3 |
485 |
4.42 x 10-5 |
VOUTSET ≥ |3%| | 129Xe |
5 |
419 |
3.84 x 10-5 |
VOUTSET ≥ |3%| |
109Ag |
1.8 |
923 |
5.13 x 10-5 |
VOUTSET ≥ |3%| | 109Ag | 3.3 |
772 |
4.31 x 10-5 |
VOUTSET ≥ |3%| | 109Ag | 5 |
650 |
3.53 x 10-5 |