SLVS861F august 2008 – june 2020 TPS40210-Q1 , TPS40211-Q1
PRODUCTION DATA
In most cases, a small filter placed on the ISNS pin improves performance of the converter. These are the components RIFLT and CIFLT in Figure 7-2. The time constant of this filter should be approximately 10% of the nominal pulse width of the converter. The pulse width can be found using Equation 10.
The suggested time constant is then
The range of RIFLT should be from about 1 kΩ to 5 kΩ for best results. Higher values can be used, but this raises the impedance of the ISNS pin connection more than necessary and can lead to noise-pickup issues in some layouts. CISNS should be located as close as possible to the ISNS pin as well to provide noise immunity.