SLVSDG2G July 2016 – December 2019 TPS2660
PRODUCTION DATA.
In this mode, during overload events, the device allows the overload current to flow through the device until I(LOAD) < I(FASTRIP). The circuit breaker threshold I(CB) can be programmed using the R(ILIM) resistor as shown in Equation 4.
where
An internal timer starts when I(CB) < ILOAD < IFASTRIP, and when the timer exceeds tCB(dly), the device turns OFF the internal FET and FLT is asserted. Once the internal FET is turned off, the device configured in latch-off mode stays latched off, until it is reset by either of the following conditions:
whereas the device configured in auto-retry mode, commences an auto-retry cycle after 540 ms. The FLT signal remains asserted until the fault condition is removed and the device resumes normal operation. Figure 41 and Figure 42 illustrate behavior of the system during electronic circuit breaker with auto-retry functionality.
MODE left floating | Load Transition from 22 Ω to 12 Ω | |
RILIM = 8 kΩ |
Load Transition from 22 Ω to 12 Ω , RILIM = 8 kΩ | ||