SLVSE94G September 2018 – June 2024 TPS2663
PRODUCTION DATA
The TPS2663x devices feature accurate overload current limiting and fast short-circuit protection feature. With TPS26630 and TPS26632, if the load current exceeds the programmed current limit, IOL, the device regulates the current through it at IOL, eventually reducing the output voltage. The power dissipation across the device during this operation is (VIN –VOUT) × IOL, and this can heat up the device and eventually enter into thermal shutdown. The maximum duration for the overcurrent through the FET tCL_PLIM(dly), 162 ms (typical). If the thermal shutdown occurs before this time, the internal FET turns OFF and the subsequent operation (auto-retry or latch-off) depends on the MODE pin configuration in Table 8-1. Figure 8-12 and Figure 8-13 illustrate overload current limiting performance.
VIN_SYS = 24 V | MODE connected to GND (Auto-Retry) | RILIM = 9 kΩ |
VIN_SYS = 24 V | MODE connected to GND (Auto-Retry) | RILIM = 9 kΩ |