SLVSEW6F August 2021 – March 2024 TPS7H2211-SEP , TPS7H2211-SP
PRODUCTION DATA
In applications where a primary and secondary (redundant) power rails are present, the TPS7H2211 readily implements cold sparing because of its reverse current blocking capability. Generally, the primary eFuse will be enabled. If there is a reason to switch to the secondary rail, the primary eFuse will be turned-off and the secondary eFuse will be turned-on. In this cold sparing application, since the eFuse is placed at the input of the point of load regulator, the on-resistance of the switch is not highly critical.