SLVSFV5B July 2023 – October 2024 DRV8262
PRODUCTION DATA
Thermoelectric coolers (TEC) work according to the Peltier effect. When a voltage is applied across the TEC, a DC current flows through the junction of the semiconductors, causing a temperature difference. Heat is transferred from one side of the TEC to the other. This creates a “hot” and a “cold” side of the TEC element. If the DC current is reversed, the hot and cold sides reverse as well.
A common way of modulating the current through the TEC is to use PWM driving and make the average current change by varying the ON and OFF duty cycles. To allow both heating and cooling from a single supply, a H-bridge topology is required. In the dual H-bridge mode, the device can drive two H-bridges to drive two TECs bi-directionally with up to 10-A current. In the single H-bridge mode, the device can drive a single TEC with up to 20-A current.
The DRV8262 also features integrated current sensing and current sense output (IPROPI) with ± 4% accuracy to eliminate the need for two external shunt resistors in a closed-loop control topology, saving bill-of-materials cost and space. The following schematic shows the DRV8262 driving two TECs.
The following schematuic shows the DRV8262 driving one TEC with higher current.
The LC filters connected to the output nodes convert the PWM output from the DRV8262 into a low-ripple DC voltage across the TEC. The filters are required to minimize the ripple current, because fast transients (e.g., square wave power) can shorten the life of the TEC. The maximum ripple current is recommended to be less than 10% of maximum current. The maximum temperature differential across the TEC, which decreases as ripple current increases, is calculated with the following equation:
Where ΔT is actual temperature differential, ΔTMAX is maximum possible temperature differential specified in the TEC datasheet, N is the ratio between ripple and maximum current. N should not be greater than 0.1.
The choice of the input PWM frequency is a trade-off between switching loss and use of smaller inductors and capacitors. High PWM frequency also means that the voltage across the TEC can be tightly controlled, and the LC components can potentially be cheaper.
The transfer function of a second order low-pass filter is shown below:
Where,
ω0 = 1 / √(LC), resonant frequency of the filter
Q = quality factor
ω = DRV8262 input PWM frequency
The resonant frequency for the filter is typically chosen to be at least one order of magnitude lower than the PWM frequency. With this assumption, Equation 20 may be simplified to -
H in dB = -40 log (fS/f0)
Where f0 = 1/ 2π√(LC) and fS is the input PWM switching frequency.
If L = 10 μH and C = 22 μF, the resonant frequency is 10.7 kHz.
This resonant frequency corresponds to 39 dB of attenuation at 100 kHz switching frequency.
For VM = 48 V, 39 dB attenuation means that the amount of ripple voltage across the TEC element will be approximately 550 mV.
For a TEC element with a resistance of 1.5 Ω, the ripple current through the TEC will therefore be 366 mA.
At 5 A current, 366 mA corresponds to 7.32% ripple current.
This will cause about 0.5% reduction of the maximum temperature differential of the TEC element, as per Equation 20.
Adjust the LC values according to the supply voltage and DC current through the TEC element. The DRV8262 supports up to 200 kHz input PWM frequency. The power loss in the device at any given ambient temperature must be carefully considered before selecting the input PWM frequency.
Closing the loop on current is important in some TEC based heating and cooling systems. The DRV8262 can achieve this without the need for external current shunt resistors. Internal current mirrors are used to monitor the currents in each half-bridge and this information is available on IPROPI pins. A microcontroller can monitor and adjust the PWM duty based on the IPROPI pin voltage.
Additionally, the DRV8262 can regulate the current internally by providing an external voltage reference (VREF) to the device to adjust the current regulation trip point. The current loop would then be closed within the H-bridge itself.