SLVUBX4A November 2020 – February 2022 LP8764-Q1
The following sections describe the various interfaces for measuring and controlling the configuration. Note: the configurations are in coordination with the settings of the PMIC. It is important to understand that both the EVM configuration and the settings of the PMIC must match. For example, if the GUI is used to change the PMIC interface to SPI from I2C, then the appropriate SPI related jumpers should be in place on J20 and J25. Please refer to the GUI User's Guide SLVUBT8 on how to update the PMIC communication protocol.