SLVUC20A March 2021 – August 2022 LP876242-Q1
The following sections describe the various interfaces for measuring and controlling the configuration. Note: the configurations are in coordination with the settings of the PMIC. It is important to understand that both the EVM configuration and the settings of the PMIC must match. The communication interface can be easily changed using the jumpers on J18 and J24. Please refer to the GUI User's Guide SLVUBT8 on how to update the PMIC communication protocol.