SLVUC28 August   2022 TPS544C26

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Description
    2. 1.2 Before You Begin
  4. 2Performance Characteristics
  5. 3Test Point Descriptions
  6. 4Test Setup
  7. 5Fusion I2C Device GUI
    1. 5.1 Opening the I2C Device GUI
    2. 5.2 On and Off Control OPERATION (01h) and ON_OFF_CONFIG (02h)
    3. 5.3 Changing SYS_CONFIG1 (A0h)
    4. 5.4 Changing the Output Voltage
    5. 5.5 Exporting and Importing Configurations
    6. 5.6 Store to and Restore from NVM
  8. 6Schematics
  9. 7PCB Layout
  10. 8BOM

Test Setup

  • A power supply capable of providing 10 A or greater must be connected to J3 (PVIN) through a pair of 14-AWG wires or better. The PVIN test points, PVIN_SNS and PGND_SNS, provide a place to monitor the PVIN input voltage. Do not use these monitoring test points as the input supply connection points. The PCB traces connecting to these test points are not designed to support high currents.
  • The load must be connected to J4 (VOUT) with a pair of 10-AWG wires or better. Wire lengths must be minimized to reduce losses in the wires. If there is too much voltage drops in the wires, then the electronic load may not be able to sink the full rated current. The VO_REG test point is used to monitor the output voltage with GND_REG as the ground reference.
  • When testing with an external 5-V bias supply to power VCC/VDRV, connect the external supply to J5 (EXTBIAS) with a pair of 20-AWG wires or better.
  • To test the VINSENP function, connect a load to J2 (IEXT) with a pair of 14-AWG wires or better. When testing this function, the PVIN power supply must be capable of sourcing this additional external load current. Additionally, the load must have the proper voltage and power rating. For example, when the voltage at PVIN is 12 V and if pulling 20 A out of J2, the power supply must also source an additional 20 A and the load must have a power rating of at least 240 W.
  • The PMBus Interface connector (J13) is provided to connect the USB-to-GPIO interface adapter to the EVM. Click here to order the adapter. The USB-to-GPIO interface adapter connects the EVM to a computer USB port which allows the Fusion Digital Powerâ„¢ graphical user interface (GUI) to communicate and control the EVM.
  • If modifications are made to the TPS544C26EVM, the input current can change. The input power supply and wires connecting the EVM to the power supply must be rated for the input current.