SLVUC32B June 2021 – February 2022 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1 , TPS6594-Q1
Change | Impact of change |
---|---|
Update NVM revision to 3, see Table 5-2. | None. |
VCCA overvoltage and undervoltage monitors are masked in the static configuration, see Table 5-8. | None. The monitors are unmasked in the PFSM once the enable pin goes high. |
BUCK and LDO overvoltage and undervoltage monitors are masked before the monitor is transitioned from the disabled to the enabled state. The corresponding monitors are unmasked just before release of the nRSTOUT/nRSTOUT_SOC. | None. These instructions are performed during the power sequences and have no impact on the timing. Additionally, the monitors are unmasked before the system can perform safety relevant functions. |
Logic and analog BIST is run at BOOT BIST, see Table 5-10. | BIST time is extended to include the logic BIST. |
For the TPS65941111, the readback interrupt for the nINT pin is unmasked. Table 5-8 | In the event of a readback error on the nINT pin, a MODERATE_ERR_INT occurs resulting in the transition to SAFE_RECOVERY. |