SLVUC39 April   2021 TPS61379-Q1

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Performance Specification
    2. 1.2 Modification
    3. 1.3 Input Capacitor C9
  3. 2Test Setup
    1. 2.1 Input/Output Connector Descriptions
  4. 3Schematic and Bill of Materials
    1. 3.1 Schematic
    2. 3.2 Bill of Materials
  5. 4Board Layout

Input Capacitor C9

The 47-uF, 25-V, tantalum capacitor C9 is added as the input capacitor in the EVM. The ESR of the tantalum capacitor is 0.12 Ω to damp the ringing of the input capacitor when the EVM is powered by a power supply with a long cable. The capacitor is not necessary and can be removed in a real application.