Note: This EVM user's guide applies to both
devices, TPSM5601R5 and TPSM5601R5S. The only difference between the two EVMs are the U1 IC
and the silk screen labeling.
Figure 1-1 highlights the user interface items associated with the EVM. The VIN Power terminal
block (J1) is used for connection to the host input supply and the VOUT Power terminal
block (J4) is used for connection to the load. These terminal blocks accept up to 16-AWG
wire.
Figure 1-1 EVM User Interface
Use the VIN S+ and VIN Sā test points along
with the VOUT S+ and VOUT Sā test points located near the power terminal blocks as voltage
monitoring points where voltmeters can be connected to measure VIN and VOUT. Do not use
these S+ and Sā monitoring test points as the input supply or output load connection
points. The PCB traces connecting to these test points are not designed to support
high currents.
Use the VIN scope (J2) and VOUT scope (J3)
test points to monitor VIN and VOUT waveforms with an oscilloscope. These test points are
intended to use un-hooded scope probes outfitted with a low inductance ground lead (ground
spring) mounted to the scope probe barrel. The two sockets of each test point are on 0.1-in
centers. Connect the scope probe tip to the top socket labeled "+" and connect the scope
ground lead to the bottom socket.
The control test points located near the
bottom of the EVM test the features of the device. Refer to Section 2 for more information on the individual control test points.
The VOUT SELECT jumper (J6) is provided to
select the desired output voltage:
1.2 V
1.8 V
2.5 V
3.3 V
5.0 V
Before applying power to the EVM, make sure that the jumper is present and properly
positioned for the intended output voltage. Always remove input power before changing the
jumper settings.
The device can be turned on or off using
the enable jumper (J5). Place the jumper in the ON position to enable the device. Place the
jumper in the OFF position to disable the device. The undervoltage lockout (UVLO) can be set
by populating resistors R1 and R2 located on the bottom side of the EVM. Refer to the data
sheet for recommended UVLO resistor values. The power good (PGOOD) test point is available
to monitor when a valid output voltage is present on the EVM. Additionally, the PG_PU pin is
present as a convenient point to connect a pullup voltage for the PGOOD signal.