SLVUCB8A May 2022 – September 2022 TPS25985
Configure the jumpers J5 and J7 positions to the desired current limits during start-up as mentioned in Table 4-3.
Configure the Jumper J6 position to desired reference voltage for overcurrent protection and active current sharing as mentioned in Table 4-3.
Enable the eFuse by releasing the switch SW1.
Observe the waveform at VOUT (TP4) and input current using an oscilloscope. The main intention of this experiment is to observe the output voltage & input current profiles and time required to complete the inrush with two different ILIM set points having all other test conditions identical. The inrush current hits the current limit set point in one case, but does not in the next.
Figure 5-5 and Figure 5-6 show the difference between the current limit and DVDT based start-up mechanisms on the TPS25985EVM eFuse Evaluation Board having two (2) devices in parallel for RILIM of 680 and RLIM2 of 680 Ω and RILIM of 402 and RLIM2 of 402 Ω respectively.