SLVUCE8A March 2022 – February 2023 TPS7H5001-SP
The following global variables are used within the F11 window of SIMPLIS. Global variables are used by the TPS7H5001-SP WCA device and changing the names in the F11 window, will cause the model not to work. Default values are placed so that the minimum and maximum values are the minimum and maximum values of the data sheet.
Parameter | Description | Default Mean Value |
Default Tol- Value |
---|---|---|---|
gmea | Model variable for the error amplifier transconductance | 1825 µS |
37 % |
Vr | Model variable for the reference voltage | 0.613 V |
1 % |
Rtt | Internal variable related to the voltage reference. Changing the equation will cause model to work improperly. | N/A |
N/A |
IDCOMP |
Model variable for CCSR parameter |
2.06 |
2.9% |
In addition to the listed model parameters, external component selection will also influence device behavior. The external components used in the default schematic take nominal values and, as such, users may see fit to add tolerances to them to model real-world variation.