Use the following instructions to perform
the power up into short test:
- Set the input supply voltage VIN to 12 V and current limit to 100 A.
Keep the power supply OFF.
- Short the output of the EVM. For example, VOUT (Connector T2) to PGND
(Connector T3) through a short and thick cable to make sure the short-circuited path
impedance is minimum as possible.
- The reference voltage for overcurrent
protection and active current sharing is at 1 V by default.
- Configure the jumpers J4 and J5 positions
to the desired current limits during start-up as mentioned in Table 4-3.
- Keep the eFuses disabled by pushing the
switch SW1.
- Turn ON the power supply.
- Enable the eFuses by releasing the switch
SW1.
Figure 5-6 shows the test waveforms of power up into output short on the TPS25990EVM with one
TPS25990 eFuse and one TPS25985 eFuse in parallel. Figure 5-7 presents the current sharing between two eFuses during start-up into short.
Note: During power-up into short, a thermal
fold-back results in the current flowing through the device being less than the calculated
value of the current limit during start-up.
Figure 5-6 Power Up into Output Short Response
in TPS25990EVM (VIN = 12 V, EN Stepped Up from 0 V to 3 V,
RILIM(TPS25990) = 665 Ω, RILIM(TPS25985) = 499 Ω,
VIREF = 1 V, and OUT Shorted to PGND)
Figure 5-7 Power Up into Output Short Response
in TPS25990EVM: Current Sharing between TPS25990 and TPS25985 eFuses (VIN =
12 V, EN Stepped Up from 0 V to 3 V, RILIM(TPS25990) = 665 Ω,
RLIMI(TPS25985) = 499 Ω, VIREF = 1 V, and OUT Shorted to
PGND)