SLVUCI4B february 2023 – may 2023 TPS7H5001-SP
The output capacitance value is picked such that there is enough capacitance for the required voltage ripple and output current load step. Equation 17 shows the calculation to find the amount of capacitance required to meet the maximum allowable voltage deviation at the output in response to a worst-case load transient. Equation 19 determines the amount of output capacitance that is needed to meet the output voltage ripple requirements of the design.