Follow these steps to design an active
filter circuit:
- Quickstart Calculator – Use
the TPSF12C1 quickstart calculator as a convenient starting point.
See Figure 3-5 for illustration.
Typical steps to complete the quickstart calculator are as follows:
- Choose the core material for
the CM chokes – the primary choices being nanocrystalline (NC) or ferrite.
NC chokes are preferable for active filter designs given their higher
permeability (and thus fewer winding turns), broader impedance
characteristic over frequency, more damped impedance behavior with softer
phase transition, and better stability over temperature.
- Define the CM choke
impedances – two options are available:
- Measure the CM
impedance magnitude and phase vs. frequency using a network
analyzer. Paste the data directly into the calculator file.
- Enter the behavioral
model parameters for each choke based on (a) a parallel LRC circuit
for a ferrite choke (LCM || RPAR ||
CPAR), or (b) a ladder network for an NC choke
consisting of three parallel RL circuits connected in series along
with a parasitic capacitance across the total network. An equivalent
circuit model is the most convenient option if the choke data sheet
includes the CM impedance data.
- Enter values for the
grid-side and regulator-side Y-capacitors, sense capacitors and inject
capacitor.
- Enter values for source
impedance of the grid supply and the noise source. Select from a drop-down
menu if a LISN (50 µH or 5 µH) is installed.
- Review the AEF loop gain plot
for stability based on the calculated component values for the damping
network. Adjust the damping network values to ensure the phase does not
reach –180° at the resonant frequencies (when the gain is positive). Refer
to the TPSF12C1 data sheet for guidance on component selection. Check the
insertion loss plots with AEF enabled and disabled.
- Circuit Simulation – Avail of
PSPICE or SIMPLIS simulation models for the TPSF12C1 device. Use such models along
with prepared test benches to investigate the operation of the complete active
filter circuit. See the SIMPLIS schematic in Figure 3-6 as an example. Perform both time-domain and frequency-domain
analyses as required.
Note that the CM choke model schematics are not shown above. If the choke
model equivalent circuit parameters are defined in the quickstart calculator,
transfer them directly to the simulation model as needed.
- Low-Voltage Tests – Validate
the filter design at low voltage prior to connecting to the switching regulator.
This is a relatively easy step to confirm various aspect of the design, including
filter stability, insertion loss, voltage swing on the INJ pin, and EMI performance
with CM signal excitation. See Figure 3-4 and refer to tests 4 through 7 described in Section 2.4.
- Insertion loss – measure with
50-Ω source and load impedances.
- Apply a CM excitation signal
with a function generator.
- Check the dynamic
voltage range of the INJ pin (TPSF12C1 pin 13).
- Measure the EMI (CM
only, there is no DM propagation in this test).
- High-Voltage Tests – Validate
the filter design while connected to the switching regulator. See Figure 3-3 and refer to tests 8 and 9 described in Section 2.4.
- Check the dynamic voltage
range of the INJ pin.
- Calculate the device power
dissipation(4) based on VVDD, IVDD, TA
and RθJA. Verify that the maximum junction temperature is less
than 150°C under the worst case operating conditions.
- Check the sense and inject
capacitance variation over temperature and ensure the circuit is stable
under all operating conditions.
- Measure the total EMI.
Separate the CM (asymmetrical) and DM (symmetrical) propagation components,
as the TPSF12C1-based AEF circuit only attenuates the CM noise.