SLVUCP8 September 2024 TPS26750
To configure additional fields and registers such as I2C Interrupt Masking, GPIO events, or making custom changes to Source/Sink PDOs, click on the Advanced Configuration slider at the top of the tool. After clicking on the slider, a message appears asking for confirmation before enabling Advanced Configuration.
Once Advanced Configuration is enabled, an Advanced Icon appears on the left side underneath the gear icon to go back to the questionnaire. Within Advanced Configuration, users have the ability to configure specific registers on the TPS26750. For details on register fields and the description, refer to the TPS26750 Technical Reference Manual. See the example below of configuring the Source_PDO_4 under Transmit Source Capabilities (0x32).