SLVUCR7 September 2024 TPS26750
The figure below shows the interface for the GPIO hardware. The register fields GPIO_AI_EN, GPIO_PD_EN, GPIO_PU_EN, GPIO_OE, and GPIO_OD_EN listed in the table below are passed along to the GPIO hardware, independent of the GPIO Event that is configured. The PD controller will then set the signal GPIO_O to high or low to implement the selected output GPIO event. So for example, each output GPIO Event is configurable as push-pull or open-drain using the GPIO_OD_EN bit. For input GPIO events the PD controller will monitor GPIO_I from the figure.
A given GPIO Event can only be assigned to one GPIO pin.
The ProcHot_N_Event GPIO Event can be assigned to any GPIO, but for some PD controllers only a specific GPIO will have the fast reaction time feature (see device data-sheet).