SLVUCR7 September   2024 TPS26750

 

  1.   1
  2.   Read This First
    1.     About This Manual
    2.     National Conventions
    3.     Glossary
    4.     Related Documents
    5.     Support Resources
    6.     Trademarks
  3. 1Introduction
    1. 1.1 Introduction
      1. 1.1.1 Purpose and Scope
    2. 1.2 PD Controller Host Interface Description
      1. 1.2.1 Overview
      2. 1.2.2 Register and field notation
    3. 1.3 Unique Address Interface
      1. 1.3.1 Unique Address Interface Protocol
  4. 2PD Controller Policy Modes
    1. 2.1 Overview
    2. 2.2 Source Policy Mode
    3. 2.3 Sink Policy Mode
  5. 3Register Overview
  6. 4TPS26750 Registers
  7. 54CC Task Detailed Descriptions
    1. 5.1 Overview
    2. 5.2 CPU Control Tasks
      1. 5.2.1 'Gaid' - Return to normal operation
      2. 5.2.2 'GAID' - Cold reset request
    3. 5.3 PD Message Tasks
      1. 5.3.1  'SWSk' - PD PR_Swap to Sink
      2. 5.3.2  'SWSr' - PD PR_Swap to Source
      3. 5.3.3  'SWDF' - PD DR_Swap to DFP
      4. 5.3.4  'SWUF' - PD DR_Swap to UFP
      5. 5.3.5  'GSkC' - PD Get Sink Capabilities
      6. 5.3.6  'GSrC' - PD Get Source Capabilities
      7. 5.3.7  'ESkC' - PD EPR Get Sink Capabilities
      8. 5.3.8  'ESrC' - PD EPR Get Source Capabilities
      9. 5.3.9  'GPPI' - PD Get Port Partner Information
      10. 5.3.10 'SSrC' - PD Send Source Capabilities
      11. 5.3.11 'MBRd' - Message Buffer Read
    4. 5.4 Patch Bundle Update Tasks
      1. 5.4.1 'PBMs' - Start Patch Burst Mode Download Sequence
      2. 5.4.2 'PBMc' - Patch Burst Mode Download Complete
      3. 5.4.3 'PBMe' - End Patch Burst Mode Download Sequence
      4. 5.4.4 'GO2P' - Go to Patch Mode
      5. 5.4.5 'FLrd' - Flash Memory Read
      6. 5.4.6 'FLad' - Flash Memory Write Start Address
      7. 5.4.7 'FLwd' - Flash Memory Write
      8. 5.4.8 'FLvy' - Flash Memory Verify
    5. 5.5 System Tasks
      1. 5.5.1 'DBfg' - Clear Dead Battery Flag
      2. 5.5.2 'I2Cr' - I2C read transaction
      3. 5.5.3 'I2Cw' - I2C write transaction
      4. 5.5.4 'GPsh' - set GPIO high
      5. 5.5.5 'GPsl' - set GPIO low
  8. 6User Reference
    1. 6.1 PD Controller Application Customization
    2. 6.2 Loading a Patch Bundle
    3. 6.3 AUTO_NEGOTIATE_SINK Register
      1. 6.3.1 AUTO_NEGOTIATE_SINK usage example #1
      2. 6.3.2 AUTO_NEGOTIATE_SINK usage example #2
      3. 6.3.3 AUTO_NEGOTIATE_SINK usage example #3
      4. 6.3.4 AUTO_NEGOTIATE_SINK usage example #4
    4. 6.4 IO_CONFIG Register
      1. 6.4.1 GPIO Events
  9. 7Revision History

National Conventions

This document uses the following conventions.

  • Hexadecimal numbers may be shown with the suffix h or the prefix 0x. For example, the following number is 40 hexadecimal (decimal 64): 40h or 0x40.
  • Registers in this document are shown in figures and described in tables.
    • Each register figure shows a rectangle divided into fields that represent the fields of the register. Each field is labeled with its bit name, its beginning and ending bit numbers above, and its read/write properties with default reset value below. A legend explains the notation used for the properties.
    • Reserved bits in a register figure can have one of multiple meanings:
      • Not implemented on the device
      • Reserved for future device expansion
      • Reserved for TI testing
      • Reserved configurations of the device that are not supported
    • Writing nondefault values to the Reserved bits could cause unexpected behavior and should be avoided.