Click on the first driver download link, ti_msp430driver_setup_1.0.1.1-windows.zip | Windows Installer.
Please log in with myTI credentials when prompted and provide the requested information. The approval to access the download is automatic and immediate as long as the U.S. Government export approval requirements are complied with.
Click on the download button to download the installer to your PC.
Double-click on the downloaded zip file and run the installer by double-clicking on the .exe file. Complete the installation to install the required USB drivers to use the EVM on the PC.
Follow proper safety precautions working with sensitive electronics as well as high voltage and high current hardware.
Power sequencing: The USB cable must be plugged in first between the EVM and the computer. Then turn on the power supply to the EVM. Powering the EVM external bench supply before connecting the USB cable can cause the USB device to not start up properly and result with driver error.
Set up the bench supply to <=40V with current limit set to appropriate requirements of the motor.