LP5899EVM is the connectivity IC between MCU and
LP589x Family LED Driver. This section provides the guidance to use LP5899EVM to
control LP5891Q1EVM by SPI.
Following the suggested jumper setting, the board can be evaluated by USB power
directly and does not need an external power supply. Single LP5891EVM can be quickly
set up and tested by following these steps:
- Following the jumper setting in
Figure 2-1 and Figure 2-2 .
-
- Connect the BoosterPack™ connectors (J5, J6, J7, J8) on the LP5899EVM
with the BoosterPack connectors (J1, J2) on the LP5891Q1EVM as shown in the
Figure 2-3.
- Connect BoosterPack connectors
(J1, J2, J3, J4) on the LAUNCHXL-F280039C with the BoosterPack connectors (J3,
J4) on the LP5899EVM as shown in the Figure 2-4.
- Power the LAUNCHXL-F280039C
through the USB cable.
- Download the code into the
LAUNCHXL-F280039C with TI Code Composer Studio™
software.