Figure 3-1 illustrates the EVM schematic.
Note: - To evaluate the performance of one TPS25984B eFuse at lower currents (< 55A), RZ5, RZ6, RZ7, RZ8, and RZ9 resistors need to be depopulated. Also R11 and R12 resistors must be populated to disable the secondary eFuse.
- The ground connections for the various components around the TPS25984B eFuses must be wired directly to each other and the GND pins of respective eFuses. This must be followed by connecting them to the system ground at one point, as implemented using RZ1 and RZ4 resistors in the EVM schematic. Do not connect the various component grounds through the high current system ground line.