Use the following instructions to evaluate the thermal performance of TPS25984BEVM:
- Configure the Jumper J6 position to desired reference voltage (VIREF) for overcurrent protection and active current sharing as mentioned in Table 4-3. The "1-2" position of the jumper J6 is selected in this experiment, which makes VIREF as 1V (typical).
- Configure the jumpers J5 and J7 in a good position to set required steady state current limit threshold (IOCP) as per Table 4-3. The "1-2" position of the jumpers J5 and J7 are selected in this experiment, which makes IOCP as 120A (typical) with VIREF as 1V (typical).
- Set the input supply voltage VIN to 12V and current limit of 115A.
- Connect the power supply between VIN (Connector T1) and PGND (Connector T3) and enable the power supply.
- Now apply a load of 110A (DC) between VOUT (Connector T2) and PGND (Connector T3) for half an hour or more to reach the thermal equilibrium point.
- Capture the thermal image of the EVM or monitor the voltage at TEMP (TP12) pin using a digital multimeter. Voltage at the TEMP (VTEMP) pin reports the maximum die temperature between two (2) TPS25984B eFuses, which can be obtained using Equation 1.
Equation 1.
Figure 5-16 shows the thermal performance of TPS25984BEVM with two (2) TPS25984B eFuses in parallel.