SLYT834 March   2023 ISOUSB211

 

  1. Introduction
  2. Existing implementation of OTG USB applications
  3. On-the-go operation
  4. Implementation of isolated OTG
  5. Demonstration of OTG with ISOUSB211 EVM
  6. Scenario A: Isolated OTG module connected to a USB-drive (bus-powered)
  7. Scenario B: Isolated OTG module connected to a laptop (host)
  8. Demonstration
  9. Connect phone to laptop
  10. 10Connect phone to USB-drive
  11. 11Summary

Demonstration

The following segment demonstrates the implementation of OTG with ISOUSB211EVM evaluation module.

To demonstrate the power delivery from A-type device to B-type device in either direction, an additional SN6505EVM was introduced.