SLYT850 February   2024 UCD3138

 

  1.   1
  2. 1Introduction
  3. 2Charge-mode control
  4. 3Control law
  5. 4RHPZ effect and solution
  6. 5Conclusion
  7. 6References

Introduction

In a control system, if you want to control something, you need to sense it; this applies to power factor correction (PFC) applications as well. In offline power supplies with power levels >75W, PFC controls the input current to create a sinusoidal waveform (in other words, following the sinusoidal input AC voltage). In order to control the input current, it needs to be sensed.

The most common current-sensing method places a shunt resistor at the PFC ground return path (designated as R in Figure 1) to sense the input current. The sensed input current signal (ISENSE) is then sent to an average current-mode controller [1] (shown in Figure 2). Because the current reference (IREF) is modulated by the input voltage (VIN), it is a sinusoidal waveform. The control loop forces the input current to follow IREF, thus achieving a sinusoidal waveform.

GUID-20240207-SS0I-6QTQ-FLKL-MNQWSC3ZHLVQ-low.svg Figure 1 A common current-sensing method for PFC.
GUID-20240207-SS0I-3Q0J-02SQ-GRJK4XSSDGFM-low.svg Figure 2 Traditional average current-mode control for PFC.

Almost all continuous conduction mode (CCM) PFC controllers use traditional average current-mode control. Although traditional average current-mode control achieves a good power factor and has low total harmonic distortion, it also has some limitations, especially in totem-pole bridgeless PFC. This article presents a brand-new control algorithm: charge-mode control [2].