SLYT853 May   2024 ADC12DJ5200RF

 

  1.   1
  2. 1Introduction
  3. 2AAF design approach
  4. 3AAF design process and parameters
  5. 4AAF design trade-offs
  6. 5AAF design example
  7. 6AAF design conclusion
  8. 7Additional resources

AAF design trade-offs

The parameters in this interface circuit are very interactive; therefore, it is almost impossible to optimize the circuit for the primary specifications (bandwidth, bandwidth flatness, SNR, SFDR and gain) without small trade-offs. However, you can minimize bandwidth peaking, which often occurs at the tail end of the bandwidth response, by varying RA, RKB, or both; either can have a net positive or net negative affect on AAF bandwidth performance.

Notice in Figure 3 how the pass-band peaking is enhanced or flattened as the value of the FDA’s output series resistance (RA) changes (the blue dashed curves). As the value of this resistance decreases, there is more signal peaking, and the amplifier can drive the signal less to fill the ADC’s full-scale input range at the cost of the pass-band flatness response near the edge of the AAF frequency response.

 Pass-band flatness performance
                    vs. RA and RKB variations. Figure 3 Pass-band flatness performance vs. RA and RKB variations.

The value of RA could also affect SNR performance. Smaller values, while enhancing bandwidth peaking, tend to decrease the SNR because of the increased bandwidth and unwanted noise.

It’s also important to select the RKB series resistor on the ADC inputs to minimize distortion caused by any residual charge injection from the internal sampling capacitor within the ADC. However, increasing this resistor also tends to enhance or reduce bandwidth peaking as well, depending on the filter topology.

When optimizing for the AAF’s rolloff frequency, varying CAAF2 by a small amount allows you to correct for optimal frequency coverage for the application.

Normally, determining the value of the ADC input termination resistor, RTADC, makes the net ADC input impedance look near typical of most amplifier characteristic load (RL) values. Selecting too high or too low a value for RTADC can have an adverse effect on the amplifier’s linearity, which will then be reflected in the overall SFDR signal-chain lineup.