The basic AAF design process and
guidelines are:
- Set the external ADC termination
resistor (RTADC) appropriately. This helps the AAF realize a “real”
impedance over its desired frequency response.
- Select RKB based on
experience or the ADC data sheet recommendations; typically, this will be
between 5Ω and 50Ω.
- Use Equation 1 to calculate the filter load impedance so that the aggregate parallel and
series combination of RTADC, RKB and RADC is
between 100Ω and 400Ω. See my recommendation in the previous
section.
Equation 1. ZAAFL -
RTADC || (RADC +
2RKB)
- Select the amplifier external
series resistor (RA). This is typically between 5Ω and 50Ω.
RA helps dampen the amplifier output response and reduce
unnecessary peaking in the pass band.
- Use the calculated
ZAAFL so that the total load seen by the amplifier
(ZAL) is optimal for the particular differential amplifier
chosen. See Step No. 1 above in the AAF Design Approach Section and use Equation 2:
Equation 2. ZAL =
2RA + ZAAFL
Keep in mind that ZAL is the
FDA’s characterized RL; therefore, using too high or too low a
value can have an adverse effect on the amplifier’s linearity.
- Calculate the filter source
resistance using Equation 3:
Equation 3. ZAAFS =
ZO + 2RA
- Using a filter design program,
design the filter using the same source and load impedances, if possible,
ZAAFS and ZAAFL. This helps reduce the amount of loss
in the filter. Any mismatch between the input/output impedance has a loss of
10*log(input Z/output Z). For example, with an input impedance of 50Ω and an
output impedance of 200Ω, the loss of the filter is –6.0dB or 10*log(50/200).
Also, using a bandwidth that is about 10% more or higher than the desired
bandwidth of the application will ensure that the intended bandwidth is covered
per the application, and help overcome any second- and third-order parasitic
losses unrealized during the filter implementation process.
After running a few
preliminary simulations, give the circuit a quick review for the following
items:
- The value of CAAF2 &
3 should be sufficiently big relative to CADC, which
minimizes the sensitivity of the filter to variations in CADC.
- The ratio of ZAAFL to
ZAAFS should not be more than 6-to-7, so that the filter is
within the limits of most filter tables and design programs. Ideally, they
should be the same to minimize loss, but this is not usually possible.
- Try to use a value of
CAAF2 in the few picofarads range to minimize sensitivity to
parasitic capacitance and component variations.
- Inductors LAAF1 and
LAAF2 should be reasonable values and in the nanohenries
range.
- The value of CAFF2 and
LAAF2 should be reasonable values; select these two parameters to
optimize the filter’s center frequency. Sometimes circuit simulators can make
these values too low or too high. To make these values more reasonable, simply
ratio these values with better standard-value components that maintain the same
resonant frequency.
- Use 0201 package styles if
possible when designing in the gigahertz range to minimize second- and
third-order parasitic effects that could disrupt the filter character shape or
outline.
In some cases, the filter design
program may provide more than one unique solution, especially with higher-order
filters. Always choose the solution that uses the most reasonable set of component
values. For filter configurations that end with a shunt capacitor, take the ADC’s
internal input capacitance into consideration as well. You may need an iteration or
two to set the filter pole and ultimate bandwidth correctly.