SLYT853 May 2024 ADC12DJ5200RF
Assuming that you have decided on the correct FDA for your application and whether to use either a low-pass or band-pass filter in order to achieve optimum performance (bandwidth, SNR and SFDR) in front of the ADC, follow these three steps:
Figure 1 shows an example of the specification table.
The generalized circuit shown in Figure 2 and filter parameter list in Table 1 apply to most high-speed differential FDA and ADC interfaces; you can use both as a basis for the AAF design.
Although not every filter construction will be exactly the same, Figure 2 can serve as a blueprint on how to kick-start your design. Using this design approach will tend to minimize the insertion loss of the filter by taking advantage of the relatively high input impedance of most high-speed ADCs and the relatively low output impedance of the driving source (the FDA).
Symbol | Parameter description |
---|---|
Ri | Amplifier input impedance |
Zo | Amplifier output impedance |
RA | Series output resistance located near the amplifier’s outputs |
RTAMP | Back-termination resistance near the amplifier outputs |
CAAF1 | First AAF capacitor |
LAAF1 | First AAF inductor |
CAAF2 | Second AAF capacitor |
LAAF2 | Second AAF inductor |
CAAF3 | Third AAF capacitor |
RTADC | Back-termination resistance near the ADC inputs |
RKB | Series kickback resistor located near the ADC’s inputs |
ZAL | Aggregate load impedance as seen by the amplifier |
ZAAFS | Aggregate source impedance of the AAF |
ZAARL | Aggregate load impedance of the AAF |