SLYY221 November   2023 ADC12DJ5200RF , ADS124S08 , ADS127L11 , AFE2256 , REF35 , REF70 , TPS62912 , TPS62913 , TPS7A94 , TPSM82912 , TPSM82913 , UCC5880-Q1

 

  1.   1
  2.   Overview
  3.   At a glance
  4.   Why high voltage?
  5.   Optimizing wide-bandgap FET performance with component innovations
  6.   Selecting the right gate drivers
  7.   Selecting the right controllers
  8.   Maximizing power density with topology innovations
  9.   Achieving extreme efficiency targets with system-level innovation
  10.   Addressing EMI challenges
  11.   Conclusion
  12.   Additional resources

Maximizing power density with topology innovations

In addition to component-level innovations, topology innovations can help you simplify power conversion in high-voltage systems. The AC/DC rectifier is a great example of how wide band-gap technologies can elevate well-known topologies to improve power density and reduce design weight. Historically, engineers used a bridge diode rectifier with a capacitor to rectify the AC voltage into the DC voltage, as shown in Figure 7.

GUID-20231004-SS0I-RD0G-GRDL-HTN9SDFJD1KS-low.svg Figure 7 A full-bridge rectifier.

The power factor of such a rectifier is generally lower than 0.5, depending on the total impedance of output capacitor and load. This is not energy-efficient, as such a design generates too much unused power (reactive power).

To solve the low-power-factor issue, engineers came up with the idea of an active power factor correction (PFC) circuit. Figure 8 shows a boost PFC circuit, which generally takes a universal AC voltage (90 VAC to 264 VAC) and boosts the voltage to a regulated 400-V voltage at the output. With input voltage sensing, the controller regulates the inductor current to follow the AC sinusoidal shape to get an almost unity power factor (0.99).

GUID-20231004-SS0I-R0LN-0LNN-XKWMB2FMCQ9F-low.svg Figure 8 Boost PFC circuit.

This type of boost PFC rectifier is able to achieve really high efficiency (>98%) with a superjunction silicon MOSFET and a SiC diode.

The full-bridge diode rectifier in the boost PFC rectifier does consume more than 1% of overall efficiency losses in kilowatt-level high-voltage systems. For example, a more than 20-W loss on a full-bridge diode rectifier is expected in a 2-kW rectifier. It is very difficult to dissipate a 20-W loss from a single device. To reduce losses on the full-bridge diode rectifier, the totem-pole bridgeless PFC shown in Figure 9 presents a good alternative. Because the rectifier function is integrated with the boost converter and has only two additional MOSFETs (instead of four diodes), the total rectifier loss (with the two low-frequency FETs) is much lower than in the original bridge rectifier example.

GUID-20231004-SS0I-S2DN-WT9K-XMLC3PK66XR2-low.svg Figure 9 A totem-pole bridgeless PFC circuit.

A continuous-conduction-mode (CCM) totem-pole bridgeless PFC is a hard-switching converter, which is widely applied in high-voltage rectifiers. Therefore, if you apply a silicon MOSFET to a totem-pole bridgeless PFC, the silicon MOSFET will suffer from high switching losses caused by Qrr. As shown in Figure 10, after the top-left MOSFET body-diode current conduction, Qrr will generate a reverse-recovery current to charge the bottom-left MOSFET Coss during the dead time of the left half bridge. Once the bottom-left MOSFET turns on, the Qrr-induced energy will dissipate into the bottom-left MOSFET. The Qrr-related loss consumes the loss reduction on the full-bridge diode rectifier.

GUID-20231004-SS0I-LXW7-JJMQ-WXBB8Z9H9BQN-low.svg Figure 10 Switching losses caused by reverse-recovery charge in a totem-pole bridgeless PFC.

The existence of wide band-gap FETs can, for the most part, help solve Qrr-related loss issues with the new totem-pole bridgeless PFC topology. A SiC MOSFET can achieve a 20 times smaller Qrr than a superjunction MOSFET with the same on-resistance level – and a GaN FET can achieve zero Qrr. When combining component and topology innovations in the rectifier example (in other words, applying wide band-gap FETs with a totem-pole bridgeless PFC), you can achieve over 99% efficiency (a >1% efficiency improvement), unlocking higher power density and lighter weight in your designs.