SLYY222 November 2023 ADC12DJ5200RF , ADS127L11 , REF35 , REF70 , TPS62912 , TPS62913 , TPS7A20 , TPS7A94 , TPSM82912 , TPSM82913
High-resolution ADCs are more sensitive to voltage reference noise, which directly impacts voltage measurements because of their direct connection to data-conversion circuitry. Ultra-low-noise voltage references help high-resolution ADCs reach their full resolution potential. The REF70 has ultra-low 1/f noise that attaches with products that require ultra-low noise such as high-resolution ADCs or a multichannel analog front end such as the AFE2256. Adding low-pass filters on the output of the voltage reference lowers broadband noise and thus lowers system noise, as shown in Figure 8.
When designing a low-pass filter, it is important to ensure that the output impedance does not degrade AC performance. This can occur in resistor-capacitor low-pass filters where a large series resistance affects the load transients caused by output current fluctuations. Choose a low-pass filter bandwidth cutoff frequency under 10 Hz to limit the impact of broadband noise.