If not already installed, then
install TICS Pro software from TI website: TICS Pro
Software GUI.
Start TICS Pro software.
Make sure the steps under Section 2.1 have been
completed before performing this step. Select the LMKDB1104 profile from
Select Device → Clock Distribution with Divider →
LMKDB1104.
Confirm communication with the
board as follows:
Click USB
Communication from the menu bar.
Click Interface to
launch the Communication Setup pop-up window.
Confirm following field
the Communication Setup pop-up window:
Make sure
USB2ANY is selected as the interface.
In case of
multiple USB2ANY, select desired interface. If a USB2ANY is
currently in use in another TICS Pro, then the user must release
that interface by changing the interface setting to
DemoMode.
Click
Identify to blink LED shown in Figure 3-1. After clicking the Identify button,
the LED flashes quickly at about 0.5 second on, 0.5 second off
for about 5 seconds. This confirms the connection to the board.
However, be aware that USB2ANY devices connected to the PC, but
not attached to a TICS Pro instance, can blink at a slow rate of
1 second on, 1 second off continuously.
Confirm all the fields match the ones shown in
Figure 3-2.