LMKDB1204EVM shows default jumper configuration for the EVM.
To begin using the LMKDB1204EVM,
follow the steps below.
- Verify the EVM default jumper as described in
Table 3-1 and LMKDB1204EVM.
- Change jumper JP9 from position 1-2 to position 2-3 to use USB supply.
- Connect the USB cable to USB port
at J13.
- Connect 100MHz reference clock to CLKIN0_P/N.
Refer to Table 4-8 for different input reference configurations.