DP83822, DP83825, and DP83826 (referred throughout this document as DP8382x) devices are a family of 10/100Mbps Industrial Ethernet physical layer (PHY) that is compliant to IEEE 802.3. This application note discusses 100BASE-TX and 10BASE-Te compliance testing and the procedures for operating the DUT for these tests.
Tektronix® is a registered trademark of Tektronix, Inc.
Spirent® is a registered trademark of Spirent Communications plc.
Agilent® is a registered trademark of Agilent Technologies, Inc.
Keysight® is a registered trademark of Keysight Technologies, Inc.
Rohde & Schwarz® is a registered trademark of Rohde & Schwarz GmbH & Co. KG.
LeCroy® is a registered trademark of Teledyne LeCroy, Inc..
All trademarks are the property of their respective owners.
Table 1-1 provides a list of terminology that is used throughout this application note.
ACRONYM | DEFINITION |
---|---|
DUT | Device Under Test |
LP | Link Partner |
PHY | Physical Layer Transceiver |
SMI | Serial Management Interface |
IPG | Inter-Packet Gap |
FLP | Fast Link Pulse |
NLP | Normal Link Pulse |
TX | Transmit – Digital Pins |
RX | Receive – Digital Pins |
TD | Transmit – Analog Pins |
RD | Receive – Analog Pins |
AVD | Analog Supply |
CT | Magnetic Center Tap |
VDDIO | Digital Supply |
BIST | Built-In Self-Test |
TPM | Twisted Pair Model |
AOI | Active Output Interface |
AFE | Analog Front-End |
MDI |
Media Dependent Interface |
MDIX |
Crossover version of Media Dependent Interface |
VoD |
Differential Output Voltage |