SNLA466A August   2024  – October 2024 DP83822I , DP83826E , DP83826I , DP83867E , DP83867IR , DP83869HM

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Abbreviation
  5. 2Introduction
  6. 3EMC Emission
    1. 3.1 Radiated Emission
      1. 3.1.1 Test Setup for Radiated Emission Test
      2. 3.1.2 Main Radiated Emission Sources
    2. 3.2 Conducted Emission
      1. 3.2.1 Test Setup for Conducted Emission Test
      2. 3.2.2 Main Conducted Emission Sources
    3. 3.3 Debug Procedure on EMC Emission
      1. 3.3.1 General Debug Procedure
      2. 3.3.2 RE Specific Debug
      3. 3.3.3 CE Specific Debug
  7. 4EMC Immunity Test
    1. 4.1 EMI Passing Criteria
    2. 4.2 Common EMI Knowledge
    3. 4.3 IEC61000 4-2 ESD
      1. 4.3.1 ESD Test Setup
      2. 4.3.2 Possible Root Cause of Failure
      3. 4.3.3 Debug Procedure
        1. 4.3.3.1 Follow the Test Setup
        2. 4.3.3.2 Remove External Factors on Cable or Link Partner
        3. 4.3.3.3 Areas to Explore to Improve ESD Performance
          1. 4.3.3.3.1 Air or Capacitive Coupling Discharge ESD Recommendations
          2. 4.3.3.3.2 Direct Contact Discharge ESD Recommendation
        4. 4.3.3.4 Schematic and Layout Recommendations
    4. 4.4 IEC 61000 4-3 RI
      1. 4.4.1 RI Test Setup
      2. 4.4.2 Possible Root Cause of Failure
      3. 4.4.3 Debug Procedure
        1. 4.4.3.1 Follow RI Test Setup
        2. 4.4.3.2 Remove External Factor on Cable or Link Partner
        3. 4.4.3.3 Found out Main Emission Area
        4. 4.4.3.4 Schematic and Layout Recommendation
    5. 4.5 IEC 61000 4-4 EFT
      1. 4.5.1 EFT Test Setup
      2. 4.5.2 Possible Root Cause of Failure
      3. 4.5.3 Debug Procedure
        1. 4.5.3.1 Follow EFT Test Setup
        2. 4.5.3.2 Remove External Factor on Cable or Link Parnter
        3. 4.5.3.3 Areas to Explore to Improve EFT Performance
        4. 4.5.3.4 Schematic and Layout Recommendation
    6. 4.6 IEC 61000 4-5 Surge
      1. 4.6.1 Surge Test Setup
      2. 4.6.2 Possible Root Cause of Failure
      3. 4.6.3 Debug Procedure
        1. 4.6.3.1 Follow Surge Test Setup
        2. 4.6.3.2 Remove External Factor on Cable or Link Partner
        3. 4.6.3.3 Area to Explore to Improve Surge Performance
        4. 4.6.3.4 Schematic and Layout Recommendation
    7. 4.7 IEC 61000 4-6 CI
      1. 4.7.1 CI Test Setup
      2. 4.7.2 Possible Root Cause of Failure
      3. 4.7.3 Debug Procedure
        1. 4.7.3.1 Follow CI Test Setup
        2. 4.7.3.2 Remove External Factors on Cable or Link Partner
        3. 4.7.3.3 Areas to Explore to Improve CI Performance
        4. 4.7.3.4 Schematic and Layout Recommendation
  8. 5Schematic and Layout Recommendation for All EMC, EMI Tests
    1. 5.1 Schematic Recommendation
    2. 5.2 Layout Recommendation
  9. 6Summary
  10. 7References
  11. 8Revision History

Follow CI Test Setup

  • Verify the cable before the attenuator (cable between function generator and attenuator) is isolated and not touching the cable after attenuator, DUT, LP, and Ethernet Cable
    • Normally the cable before the attenuator carries noise with huge amplitudes, easily disturbing other signal lines
  • Verify the link partner’s RJ45 shield is connected to earth ground
    • Normally the long cable is on the link partner side. There can be higher impedance between shield and earth ground if the only connection between cable shield to earth ground is within CDN. Therefore, providing a small impedance path to ground helps with CI testing
    • If the RJ45 shield is not able to connect to earth ground for the application, connect the RJ45 shield or connector ground directly to a metal or conducted case to provide a better radiated path for EMI noise to flow and radiate to the surrounding area.
  • Longer cable is preferred on the link partner side to reduce the effect on link partner
  • Verify the cable type matches on both sides of the CDN
  • Verify the CDN type matches with the cable types used
    • Mismatching unshielded cable CDN with a shielded cable can potentially increase reflective noise due to the discontinuous of ground in the signal lines
    • Using unshielded cable CDN with shielded cable can also increase the impedance of the return path between signal lines and earth ground, introducing higher amplitude noise on the signal lines
  • Verify the CDN is connected to the earth ground
  • Prevent any cable looping that can increase crosstalk
  • Verify the cable is not touching any noise source
  • Shielded cable is recommended. (CAT 6 cable preferred)
    • Having a shielded cable is better than non-shielded cable since the shielded cable provides a path from MDI lines to ground inside the CDN for through capacitors
    • For unshielded cables, all noise can go directly to the signal lines, with no noise coupling to ground