Confirm the earth ground
connection of the ESD test setup
Verify the ESD gun is
properly connected to earth ground
Verify the power supply
is connected to earth ground
Verify table ground is
properly connected to earth ground through a 1MOhm termination
Verify there is a connection
between connector ground and earth ground on both DUT and LP boards
Provide a return path for
each ESD strike to flow to earth ground, preventing the connector ground
from capacitively charging. Without a good return path for ESD noise,
the connector ground can gain charge and worsen ESD performance. This is
also dangerous for ESD testing, as significant charge can build and
discharge to testers.
Figure 4-4 Low Impedance Ground
Path
If the application prevents the RJ45 shield from connecting to earth
ground, the recommendation is to connect the shield to a metal or
conducted case (bigger conducted area) to provide a better radiated path
for ESD noise to flow
Verify the PHYs, power supply,
and Ethernet cable are placed on top of the insulator
This prevents noise from
earth ground directly interfering with the system
Use a shielded cable for improved
EMI performance
CAT6 cables have better
performance than CAT 5E cables