SNLS461A May 2013 – June 2015 DS110DF111
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The DS110DF111 is a 2 channel retimer that support many different data rates and application spaces.
Figure 9 shows a typical implementation for the DS110DF111 in a back plane application. The DS110DF111 can also be used for front port applications. The DS110DF111 supports data rates for CPRI, Infiniband, Ethernet, Interlaken and other custom data rates. For applications which include a lower VCO/4 or VCO/8 data-rate the CTLE value will not adapt automatically. Instead the CTLE value is taken directly from channel register 0x3A. For short, low-loss channels this value should be adjusted as indicated in the Channel Register Table.
This section lists some critical areas for high speed printed circuit board design consideration and study.
To begin the design process determine the following:
Initialization Sequence: Channel Register Configurations repeated for all desired channels:
Testing for Receiver Jitter Tolerance based on SFF-8431 section D11.
The SFF-8431 specification combines deterministic, random, and periodic jitter components. The combination of these jitter components has been measured and calibrated to ensure adequate levels of individual jitter components and total jitter.
The SFF-8431 specification defines a transmit eye mask to ensure robust signal reception across the host - module interface.