SNLU289 September 2020 DP83TG720R-Q1 , DP83TG720S-Q1
To Update the Software that runs on the MSP430 on the Media Converter there is the Software UNIFLASH available. The Software can be downloaded from:
http://www.ti.com/tool/UNIFLASH.
The User’s Guide can be found here: http://downloads.ti.com/ccs/esd/uniflash/docs/latest_qsguide.html.
The MSP430 Launchpad including the eZ-FET can be used as a Programmer for external MSP430 devices, and so, the MSP430F5528 can get programmed on the 720 Media Converter.
http://www.ti.com/tool/MSP-EXP430F5529LP.
Launchpad preparations:
Remove all stock jumpers marked in blue and connect as stated in this table:
Launchpad | 720 Media Converter |
---|---|
GND | GND |
SBW TST (SBWTCK) | TST |
SBW RST (SBWTDIO) | RST |
Connect the MSP430 Launchpad and the 720 Media Converter to the Computer and open UniFlash.
UniFlash should now Auto-Detect the MSP430F5528.
Click Start.
Now browse for the Flash File :
Press load image to flash the file to the MSP430F5528 on the 720 Media Converter.