SNLU301 November   2021 SN75LVPE5412 , SN75LVPE5421

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Features
    2. 1.2 Applications
  3. 2Description
    1. 2.1  Redriver-Mux 5-Level I/O Control Inputs
    2. 2.2  Redriver-Mux Modes of Operation
    3. 2.3  Redriver-Mux SMBus or I2C Register Control Interface
    4. 2.4  Redriver-Mux Equalization Control
    5. 2.5  Redriver-Mux RX Detect State Machine
    6. 2.6  Redriver-Mux DC Gain Control
    7. 2.7  DS320PR412-421EVM Global Controls
    8. 2.8  DS320PR412-421EVM Downstream Devices Control
    9. 2.9  DS320PR412-421EVM Upstream Devices Control
    10. 2.10 Quick-Start Guide (Pin Mode)
    11. 2.11 Quick-Start Guide (SMBus Slave Mode)
  4. 3Schematics
  5. 4PCB Layouts
  6. 5Bill of Materials

Quick-Start Guide (SMBus Slave Mode)

Configure all devices to operate in the SMBus Slave Mode by setting their MODE pins to the L1 level, each redriver is assigned a unique SMBus secondary address. This is accomplished by placing shunts as shown in Table 2-11.

Table 2-11 SMBus/I2C Mode Shunt Configuration
SHNT#HEADERSHUNT ACROSS PINS
1J1 - J41-2
2JMP71-2
3JMP82-3
4JMP172-3
5JMP182-3
6JMP192-3
7J171-2, 3-4
8J181-2, 3-4
9J191-2, 3-4
10J201-2, 3-4
11J211-2, 3-4
12JMP15-6
13JMP23-4
14JMP33-4
15J309-10
16J239-10
17JMP47-8
18JMP53-4
19JMP63-4
20J249-10
21J259-10
22JMP91-2
23JMP101-2
24JMP113-4
25J269-10
26J279-10
27JMP143-4
28JMP151-2
29JMP163-4
30J289-10
31J299-10
  1. Connect USB2ANY or Aardvark Adapter to P4 (Note that the Adapter is not supplied with the DS320PR412-421EVM). Install shunt on JMP17 across pins 1-2 for USB2ANY, 3-4 for Aardvark.
  2. Install SigCon Architect Version 3.0.0.16 application and the DS320PR412-421 profile.
  3. Plug the EVM into a PCIe x16 server motherboard slot. Ensure the motherboard is powered down before installing the EVM or configured for hot-plug operation.
  4. Install a compatible PCIe endpoint card into the straddle connector of the EVM.
  5. Power-up the motherboard.
  6. Start the SigCon Architect application.
  7. Select the DS320PR412-421 Configuration Page and select the Apply box to enable the device profile. If necessary, edit device addresses in the Edit Device Addresses box.
  8. In the DS320PR412-421 High Level Page, select Block Diagram as shown in Figure 2-1.
  9. Select desired EQ Settings and Driver VOD.
  10. Select the devices to which you want to apply the selected settings and click the Apply to All Channels button.
GUID-20210507-CA0I-JX10-14N6-FLGXWF0RBJ2B-low.jpgFigure 2-1 SigCon Architect DS320PR412-421 High Level Page