SNLU342 December 2023 MCT8315Z
The MCT8315ZEVM comes automatically populated with and configured for the MCT8315ZH. The EVM is also compatible with the MCT8315ZR and MCT8315ZT variants, see Section 2.7.1 for MCT8315ZT compatibility and Section 2.7.2 for MCT8315ZR compatibility.
This document is provided with the MCT8315Z evaluation module (EVM) as a supplement to the MCT8315Z data sheet. This user's guide details the hardware setup instructions, GUI installation, and usage instructions.
Hot surface temperature
The EVM can have high surface temperatures marked by the FIRE triangular symbol on the EVM. Avoid touching the marked hot surface are when driving high currents to prevent potential burn damage.