SNOA961A February 2017 – February 2023 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
The COM pin can drive a load of up to 20 nF to ground. CCOM should be sized so that the following relationship is valid for all channels.
This requirement is still necessary even if CSENSOR is not the same value for all channels.