SNOA961A February 2017 – February 2023 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
In general, the sensor capacitance is selected after the inductor has been designed, and is used to set the sensor frequency. Use of very small sensor capacitances should be avoided so that any parasitic capacitance shifts do not affect operation. As a general guideline, use of sensor capacitances smaller than 22 pF should be avoided.