SNOA961A February 2017 – February 2023 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
The sensor coils can be mounted to the metal target in many ways. The sensor mounting technique must provide consistent performance with minimal crosstalk between neighboring buttons. This implies that any force outside the button region should cause minimal local metal deflection at that button location. In order to achieve this goal, the spacer should provide robust attachment between the metal and coil. At the same time, the sensors should be mass-production friendly in terms of both cost and installation effort.
Three different mounting techniques are presented below, namely adhesive-based, spring-based, and slot-based.