SNOA963B February 2020 – July 2021 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
This example configures one of the buttons on inductive touch-cell-phone demo to trigger at 100 g of force. Figure 4-1 shows the cell-phone reference design, which employs two inductive touch buttons on each of the two side walls.
Each individual button region is 8 mm long and 6 mm tall and is constructed out of 0.4-mm thick aluminum. The inductive sensor is a flexible printed circuit board with an 8-mm long and 2.6-mm tall coil region. The sensor is separated from the cell phone side wall by an approximately 0.15-mm air gap (DTARGET = 0.15 mm).
This example configures the button that corresponds to the sensor that is connected to channel 0 on the LDC2114, and can be replicated using the LDC3114 as well. The following steps to configure the button activation force assume all the settings (power mode, scan rate, sampling window, and sensor configuration) except GAIN0 for the LDC2114 onboard the reference design have been configured correctly:
The GAINnFACTORNEW can now be correlated to a GAIN value of 40 using Table 41 in the LDC2114 datasheet (GAINnFACTORNEW was rounded up to 32 to match the closest gain factor in the table).
After the completion of step 12 the button is programmed to trigger to an activation force of 100 g. This can be verified by applying 100 g of force on the button and ensuring that OUT0 toggles, which indicates a button press.